Part Number: TCA9539-Q1
Hi, Support Team
We will use TCA9539-Q1 as below chart. have any concern?

if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9539-Q1
Hi, Support Team
We will use TCA9539-Q1 as below chart. have any concern?

if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Pulling the /RESET input to ground prevents the device from working.
If the /INT output is not used, it can be left open; pulling it to ground does not make sense.
There must be pull-up resistors on the SDA/SCL lines. I guess they are on some other part of the schematic.
Please explain the resistors at A0/A1. In the configuration shown, they short the supply to ground.
Hi Lawrence,
I agree with Clemens on most of his comments.
Pulling the /RESET pin to GND prevents the device from working. /RESET is an active-low reset, and will keep the device in a reset condition as long as it is held LOW. To have proper operation, I suggest pulling this pin to VCC through pull-up resistor, and have a GPIO connected to it so there is an option to perform an external reset by driving the pin LOW.
If /INT is not used, you can leave this pin open.
Please ensure that there are pull-up resistors present on the SDA/SCL lines. I2C is an open-drain protocol.
P-Ports that are left as outputs can be left floating. If p-ports are configured as inputs, please tie to VCC or GND through a resistor.
A0/A1 connections don't make sense since two sets of 0ohm resistors are pulling to VCC and GND. Are some of these 0 ohm resistors not-populated?
Regards,
Tyler