Part Number: TUSB8042A
Hi ,
Would like to confirm with you the feature to enable/disable DSP is dynamic or not? Or the USB hub should be reset after override the register by I2C?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The TUSB8042A supports a serial interface for configuration register access. The device may be configured by an attached I2C EEPROM or accessed as a slave by an external SMBus master.
For I2C, the TUSB8042A supports a single-master, standard mode (100 KHz) or fast mode (400KHz) connection to a dedicated I2C EEPROM when the I 2C interface mode is enabled. In I2C mode, the TUSB8042A reads the contents of the EEPROM at bus address 1010000b using 7-bit addressing starting at address 0. The TUSB8042A reads the entire EEPROM contents using a single burst read transaction. The burst read transaction ends when the address reaches FFh.
When changing the port configuration, USB hub must do a power on reset in order to read the updated EEPROM contents.
Thanks
David