Part Number: DP83867IR
Other Parts Discussed in Thread: AM3358
Hi
What is the main function of marked PHY1_RX1588 and PHY1_TX1588 lines ? In custom board, can I connect these pins to any GPIO pin of AM3358 ?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The primary use case of RX_D5,6 are for GMII MAC interface. They are also used for bootstrapping the PHY for Force MDI/X, Duplex, auto-MDIx enable, and RGMII enable.
Sincerely,
Gerome
Thanks for the reply. Can I connect these pins to any GPIO of the processor ? Is there any special input type for these signals ?
Hello,
These are typically CMOS level output pins. I would recommend seeing what capabilities the processor has and understand if GMII can be connected to it.
Sincerely,
Gerome