For this question, I am specifically referring to setup/hold violations associated with the TA[6:0] and TB[6:0] pins (parallel inputs).
I have an application that uses a bank of SN75LVDT1422 devices to transmit data from a parallel bus to an FPGA. Some of the bits on that bus are asynchronous to any clocks in the system, thus violations of the SN75LVDT1422 setup/hold times on the TA[n]/TB[n] pins are inevitable. Does Texas Instruments have any literature or information on the failure modes of the SN75LVDT1422 when these violations occur?
One obvious failure mode is that the bit in the serial stream associated with the TA[n]/TB[n] pin that violated the timing spec would be in the "incorrect" state. This failure mode is not a problem in our application.
Are there any other failure modes, such as "corruption of adjacent bits", lockup, or "serial transmitter timing violations"?