Part Number: TLIN1021A-Q1
Hi Team,
TLIN1021A have certification ISO 17987–4 electrical physical layer (EPL) specification is the same as 17987–7?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLIN1021A-Q1
Hi Team,
TLIN1021A have certification ISO 17987–4 electrical physical layer (EPL) specification is the same as 17987–7?
Kevin,
ISO 17897-7 is the specification defining the conformance test for ISO17987-4 to make sure the LIN transceiver is compliant to the physical layer specification (ISO 17897-4). So, the LIN certification to ISO17987-4 comes from the test(s) defined in ISO17897-7.
Regards,
Eric Hackett