Part Number: DS90UB960-Q1
Hi team,
1.SoC side 960 is connected with 3M camera Serializer 953, the mode of 960 is configured as CSI-2. Am I right? If I would like to use 933 which is YUV video format to connect with 960. should I use RAW mode as below pic? and how do I judge which RAW mode I can use because there has RAW12 Low Frequency Mode, RAW12 High Frequency Mode and RAW10 Mode three different modes here. Follow the previous question if I use a 1Mp camera and a 3Mp camera with 933 and 953 then connect to 960. how do I judge which FPD3_MODE I can use?

2. GPIO of 960 can be used for SYNC input and LOCK output. The LOCK output can be configured according to the register as
. My question is that Can 953 GPIO input signal send to 960 GPIO output? and Can it use multiple channels for this behavior?
BR,
Jimmy