Other Parts Discussed in Thread: SN65LVDS104, SN65LVCP22, DS25CP152
You have any one lvds input to two lvds output bridge?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65LVDS104, SN65LVCP22, DS25CP152
You have any one lvds input to two lvds output bridge?
Hello Sathiyan,
Another option could be the SN65LVCP22. It's a cross point LVDS in a 2X2 configuration and can be used as a splitter.

Regards,
Josh
Thanks Josh, Whether i can connect two lvds display using above SN65LVCP22? what i need to do SEL1/0, EN0/1 pins.
Hello Sathiyan.
If using the device in a 1:2 Splitter configuration, then use the following:
If using Input 0, then make SEL0 and SEL1 = 0
If using Input 1, then make SEL0 and SEL1 = 1
Function table and block diagram can be found on page 2 in the datasheet. Hope this helps.
Regards,
Josh
Hello Sathiyan,
That's correct. In this mode the device is essentially a fanout.
Regards,
Josh
Hello Sathiyan,
No, a fanout means you are distributing the input signal to other outputs. The SN65LVCP22 is a buffer since it's a differential to differential device.
Regards,
Josh
Everything are LVDS still need Noise Margin Analysis,
iMX6 - LVDS Splitter - O/P1 LVDS Display
-O/P2 LVDS to RGB Converter
Hello Sathiyan,
Unfortunately, we don't have any noise margin analysis for any of our LVDS devices.
Regards,
Josh
Hello Sathiyan,
The schematic looks good.
For the unused differential inputs [Input 0] I would recommend to tie the "+" input to VCC and the "-" input to GND.
Regards,
Josh
Thanks Joshua, Can i use 0 ohm or 100 ohm or 10K ohm for the unused differential inputs.
Thanks Joshua, TI having any LVDS Isolator Solutions?, I am in need isolate two LVDS Chips.
Hello Sathiyan,
Yes we do have a few isolated LVDS buffers. Take a look below.

Just note these products don't fall under my team so if you need additional information on isolated LVDS buffers, then I can redirect your question to the isolation team.
Regards,
Josh
Hello Sathiyan,
Use high-frequency, ceramic, 0.1-µF and 0.01-µF capacitors in parallel at the power supply pin with the smallest value capacitor closest to the device supply pin.
Regards,
Josh
Thanks Josh, SN65LVCP22 will support 4K and 1080p Video, I am using conversion after lvds spillter, to connect to monitor, DS25CP152TSQ/NOPB is better part compare to SN65LVCP22? Because i little bit varied about transmitted speed.
Hello Sathiyan,
SN65LVCP22 and the DS25CP152 are very similar devices. Aside from some minor spec changes, the main difference is the data rate of the DS25CP152. If the data rate you need is higher than 1 Gbps then I would recommend the DS25 device.
Regards,
Josh
Hello Sathiyan,
I'm not sure if I understand your question.
Regards,
Josh
Hello Sathiyan,
Are you asking if the SN65LVCP22 is active as in purchasable? Then the answer is yes.
Regards,
Josh