This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVPE802: Regarding to the input signal

Part Number: SN75LVPE802

Hello team,

I received a question from the customer regarding to the input signal.

Are there any numerical specifications regarding the input signals (pin 1/2, pin 12/11), and if so, what are the specifications on the input side that would guarantee that the output waveforms would meet the PCIExpress specifications?

For example, should the following requirements be required to be met as input signals to the SN75LVPE802? Please let me know if there are any other requirements that should be met.

[1] Amplitude (e.g.: Eye height: 25mVpp or more)

[2] Rise/Fall time (e.g.: xx[ps] or more)

[3] Jitter (e.g.: Tj:xx[ps]、Dj:xx[ps]、Rj:xx[ps])

[4] Other: 

Regards,

Masa