Part Number: THVD1424
When using the THVD1424 in Half-Duplex mode, are collisions on the Z/Y TX/RX pins controlled automatically internal to the IC, when I can just keep both the TX and RX enabled all the time? Or do I need to use SW control (on /RE and DE pins) to enable TX / disable RX when transmitting, and enable RX / disable TX when receiving?