Hi, expert
As title description, we study DP83TC812R driver, and found it includes two PHY_ID code.
#define DP83TC812_CS1_0_PHY_ID 0x2000a270
#define DP83TC812_CS2_0_PHY_ID 0x2000a271
static const struct dp83812_init_reg dp83812_master_cs1_0_init[] = {
{0x523, 0x0001},
{0x800, 0xf864},
{0x803, 0x1552},
{0x804, 0x1a66},
{0x805, 0x1f7b},
{0x81f, 0x2a88},
{0x825, 0x40e5},
{0x82b, 0x7f3f},
{0x830, 0x0543},
{0x836, 0x5008},
{0x83a, 0x08e0},
{0x83b, 0x0845},
{0x83e, 0x0445},
{0x855, 0x9b9a},
{0x85f, 0x2010},
{0x860, 0x6040},
{0x86c, 0x1333},
{0x86b, 0x3e10},
{0x872, 0x88c0},
{0x873, 0x0003},
{0x879, 0x000f},
{0x87b, 0x0070},
{0x87c, 0x003f},
{0x89e, 0x00aa},
{0x523, 0x0000},
};
static const struct dp83812_init_reg dp83812_master_cs2_0_init[] = {
{0x523, 0x0001},
{0x81C, 0x0fe2},
{0x872, 0x0300},
{0x879, 0x0f00},
{0x806, 0x2952},
{0x807, 0x3361},
{0x808, 0x3D7B},
{0x83E, 0x045F},
{0x834, 0x8000},
{0x862, 0x00E8},
{0x896, 0x32CB},
{0x03E, 0x0009},
{0x01f, 0x4000},
{0x523, 0x0000},
};
Each ID has its own init sequence, so what's the difference?
Does DP83TC812RRHARQ1 return "DP83TC812_CS1_0_PHY_ID" or "DP83TC812_CS2_0_PHY_ID"?
Many Thanks
Gibbs