Part Number: TPD4E05U06
Other Parts Discussed in Thread: DP83822I, STRIKE, , ESD204
Dear Specialists,
My customer is considering TPD4E05U06DQA and has a question.
I would be grateful if you could advise.
---
The breakdown voltage of TPD4E05U06DQA is 6.5V to 8.5V.
On the other hand, the absolute maximum rating of the TX± and RX± terminals of “DP83822I” is 6V.
When overvoltage is input, a voltage exceeding the absolute maximum rating (6V) is applied to the TX± and RX± terminals of the DP83822.
That won't be a problem will it?
ーーー
I appreciate your great help in advance.
Best regards,
Shinichi