Part Number: SN65LBC174A-EP
Other Parts Discussed in Thread: SN65LBC173A-EP, SN74LVC1G17-EP
Need following clarifications:
- What is the input/output capacitances and Impedance for input pins for IC: SN65LBC174A-EP?
- Do you have reference for power loss calculation for IC: SN65LBC174A-EP if using 1 channel of the IC?
- What is the input/output capacitances and Impedance for input pins for IC: SN65LBC173A-EP?
- Do you have reference for power loss calculation for IC: SN65LBC173A-EP if using 3 channel of the IC?
- For buffer IC: SN74LVC1G17-EP, if supply voltage Vcc is 3.3V will there be an issue if 5V signal is given as input at pin A?