Part Number: TUSB211A
Other Parts Discussed in Thread: TUSB211
Hi experts,
(1) I understand the following in each figure of TUSB211A data sheet 8.2.3. Figure 8-3 shows the case without TUSB211A, Figure 8-4 shows the case when TUSB211A is connected to a pre-channel cable of the same length, and Figures 8-5 and 8-6 are the same. Is this my understanding correct?
(2) It is my understanding that data sheet 8.2.3 of TUSB211 was also measured using the same setup as (1). Comparing this with each figure in 8.2.3 of the TUSB211A data sheet, if (1) is correct, the TUSB211A appears to have improved the rise/fall speed variation or jitter that existed in the original signal. Is such an understanding correct?
Thank you for your help.
Regards,
Taito \Takemura