Part Number: DS90UB949-Q1
Hello,
I am trying to use the GPIO registers between 948->949. After setting 0x0D[3:0] = 0x5 on 949 and 0x1D[3:0] = 0x3 on 948, where do I read the input? Is there a register value that will toggle for me to obtain the input value? And to confirm, this input value can be remote right? For example, I can use the 948 as a remote input value and read the value on the 949 side?