Other Parts Discussed in Thread: TCAN2450-Q1
When connecting 6-Wire SPI, can I use the SW Pin or GFO Pin of TCAN2450-Q1 as SPI_RDY_N?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TCAN2450-Q1
When connecting 6-Wire SPI, can I use the SW Pin or GFO Pin of TCAN2450-Q1 as SPI_RDY_N?
Joonggeon,
The TCAN2450-Q1 does not have a specified SPI READY signal. The SW pin is used to enable/disable the watchdog via programming mode. The GFO pin is controlled via SPI or device state, so this would not be related to the SPI status.
The TCAN24xx-Q1 supports 4-wire SPI using nINT, SDI, SDO, and CLK.
Best,
Danny