Part Number: TCAN1145-Q1
1.Does this current refer to the additional current consumed by the chip when the external bus is in operation when the selective wake-up function is enabled in sleep or standby mode?

2.If we do not use a local wake-up pin (WAKE pin), is it directly connected to ground or grounded through a resistor? What is the recommended value for resistance?
3.Does the WAKE pin allow direct connection to the 5V GPIO pin of the MCU? The MCU is Infineon TC3xx.
4.Can we achieve full state jump and operation through SPI when we do not use WAKE pins? For example, power on=>Normal Mode, Normal Mode=>Sleep Mode, etc.
Among them, VSUP is 12V normally charged, and VCC/VIO is powered down when the controlled 5V power supply is dormant.