Part Number: TLK2711-SP
Hello,
I have a question about the TLK2711-SP’s expected power dissipation. In the recommended operating conditions section, there is a nominal current draw for various operating conditions. Normally I’d expect recommended operating conditions to only include minimum-maximum ranges (i.e. stressing parameters).
Ultimately I’m interested in a current budget for our application, and how to interpret these numbers. Do the reported currents here represent current into the supply pin before accounting for capacitive loads driven by the TLK? I can see the relation between the currents and powers listed, but as for the 550 mW figure – for example, does this mean (550 – 400 ) = 150 mW is the budget for driving capacitive loads @ 2.5 Gbps?
Thanks,
Adam