Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Dear team,
My customer would like to split their application to 1G/100M/10M and 100M/10M mode due to cost reduction.
They want to use same schematic and They only want to change the magnetic and RJ45 connector.
1. Is it available to use the DP83869HM and the 100M dedicated connector(2 pair, 4 line)?
2. If they are using DP83869HM as only 100M/10M mode, Do they only need to connect port A and B to the RJ45 connection?
3. If yes, How do I handle the C and D port? floating is ok or not?
Please let me know your opinion regarding above customer questions.
Thank you.