Hi TI expert
Is there a time sequence diagram of mipi that can be provided, similar to the attached picture
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI expert
Is there a time sequence diagram of mipi that can be provided, similar to the attached picture
Hi Albert,
I am unclear on the request here. Are you asking for a timing diagram from a MIPI DSI source? What exactly are you trying to do?
Best,
Shu
Hi Yao Jun,
Do you have a specific DSI source you're using? The timing diagram should adhere to the MIPI DSI standard and it is not something we support. I recommend reaching out to the DSI generator vendor and discuss the settings with them or obtain a copy of the DSI standards to get the correct timing sequence.
Best,
Shu
Hi Yao Jun,
The timing parameters listed typically come from a display panel/LCD and can be found in their datasheet. The 941 does not generate these parameters.
The DSI source needs to be programmed with the supported timing of the LCD to transmit video to the 941. Below is the 941 DSI Bring Up Guide that provides a walkthrough of some example bring up scenarios.
Do you have a specific DSI video mode you are configuring for? The available modes are:
• Non-burst mode with sync pulses
• Non-burst mode with sync events
• Burst mode
The only initialization needed for the 941 are the DSI configurations associated with the above modes. I can help with the sample code if you know which mode the DSI Source is using.
Best,
Shu