This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP41013: Add USB-C data transmission to USB-C USB-PD (TPS25750)

Part Number: PMP41013
Other Parts Discussed in Thread: TPS25750

Where PMP41013 exhibits USB-C USB-PD via TPS25750, 
there is no exhibition of additional alternative use of the port for data transmission.

Below, the SSTX/SSRX pins are simply left floating:

If I want to use the port principally for power source/sink (as PMP41013 intends),
but alternatively for USB MCU bootloading or USB flash drive access, 
what additional circuitry would be necessary for data transmission?

Could a reference design be suggested (which would be compatible alongside TPS25750)