Part Number: TUSB8042A
Hello,
I am currently designing carrier board for Orin NX with TUSB8042A for USB SS hub.
Please correct me if my understanding is wrong.
For power sequencing requirements, VDD33 and VDD can have any sequence, as long as GRSTz is held low until at least 3ms after both VDD33 and VDD are stable.
This seems to match the way the EVM is designed, with 1.1V supply chained off of 3.3V supply, and a 1uF capacitor to ground that charges to 2V (VIH, min) in > 3ms. When power is supplied, GRSTz starts low, and then is charged through the PU resistor until GRSTz is high, enabling the controller.
However, my confusion is that the second half of note 1 in timing requirements section states that if only a capacitor is connected from GRSTz to GND, then an external signal is required to trigger GRSTz. This is in conflict with the first half of the statement and in conflict with how the EVM is designed.
Furthermore, the language for GRSTz is very confusing. The pin description states that if GRSTz is asserted, then the IC is disabled. But GRSTz is active low, which means that normal operation should have GRST_N asserted, which means GRST is low.
Please advise, thank you.