Part Number: PCA9518

I am facing a weird issue, I am connecting ATMEGA128 (running on 5v VCC) to PCA9518 through TSX0102 for both SCL & SDA lines. the PCA9518 is included to buffer I2C communication between ATMEGA128 and four other boards. The SCL0 & SDA0 are 3.3v, while all other ports are 5v (pull-up resistors connected to 5v). SCL signal can be seen on all ports, but with lower frequency than targeted (66.2KHz instead of 100KHz) and SDA is always zero logic on all port no matter which one is enabled.
I am suspecting the cause to be one of the following:
1. Using PCA9518 in series with TSX0102 rise time accelerator which might be incompatible.
2. Using large bypass capacitors connected to VCC (3.3V) one 10 uF tantalum in parallel with 0.1 uF MLCC.
3. Connecting EXPSCL1&2 EXPSDA1&2 pull-up resistors to 5V.
4. Connecting all EN to 5v logic signals.
5. Not connecting extra pull-ups at the TSX0102 outputs.
attached is part of the schematic regarding this point.
Please can anyone assist in diagnosing the cause of the issue.