Other Parts Discussed in Thread: DS90UB941AS-Q1
Hi,
We have been trying to quantify the limitations on video data rate imposed by the SerDes interface.
Our basic setup is a DS90UB941AS-Q1 paired with a DS90UB924-Q1.
The DS90UB924-Q1 datasheet suggests it can only support 720p video (section 1).
But my calculations (based on similar calculations in this forum) show it can support up to 1080p:
1920 x 1080 x 30 (fps) x ~1.2 (blanking) = 88MHz.
This is within the 95MHz pixel clock specification of DS90UB924-Q1 (section 1).
Have I understood this correctly?
Related question: Where does colour depth (e.g. 24 bit per pixel) become involved? I would have guessed this would be part of the same calculation, but the result then becomes 2.1Gbps. Is this now representative of the FPD line rate? If so, again it appears to be within the datasheet specification of 2.976 Gbps (section 7.3.1). Have I understood this correctly?
Are there any misunderstandings here, and are there any more stringent limitations placed by the SerDes set (e.g. MIPI DSI rate at the serialiser)?
Kind regards
Laurence