This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Absolute MAX current on MDC input pin / Any issue on MDC pin with external pull-up?

Part Number: DP83822I

Hi,

Could you please let us know the Absolute MAX current on MDC pins?

Also, when MDC line is connected with external pull-up (10kohm), voltage on MDC line become about 1.56V after power-up, because MDC internal pull-up register is 9kohm (Typ).  Does DP383822 occur any issues?   Please advise us.

Thanks and best regards,
M.HATTORI.