Part Number: DP83867E
Hi team,
Q1: Is the Mac Interface of the DP83867ERGZT compatible with RGMII-ID?
The following application note describes RGMII v2.0, so it probably supports it.
Please tell me just in case.
■ Application Report SNLA243 – October 2015
RGMII Interface Timing Budgets
Q2: If you want to use the Mac Interface of the DP83867ERGZT with RGMII, if the MAC side supports RGMII-ID,
is it better to set the MAC PHY mode to RGMII-ID?
Regards,
Ohashi