Part Number: DS250DF230EVM
Other Parts Discussed in Thread: DS250DF230
Hi, I'm using the DS250DF230EVM and the SigCon Architect software to evaluate DS250DF230. In order to use the PRBS Gen/Checker on the software,
I should input a signal to the retimer's RX, my question is if I want to get a 10Gpbs pattern, what's the minimum sub-rate allowed at the input?
For example, if a 500M clock signal input to the RX, can a 10.3125 Gbps PRBS signal will be generated?
Thanks,
Jochen