Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: ALP,
Customer is running some bench tests with DS90UB947 EVM and DS90UB948 on their display deserializer board connected to a display. They have three different deserializer board designs, all using the 948 DES. All three designs work in the actual final product with 947 and 949 serializers.
For the bench tests, they are using the ALP tool to command the 947 pattern generator to send a pattern to the display. This worked as expected on one of the three deserializer board designs. On the other two boards, an initial link is not established and the ALP tool does not show the 948 DES on the Information tab.
What does the DES need to do in order for the SER to auto detect it? Could they have something set wrong on these deserializer boards to cause detection to fail?