Part Number: DS90UB941AS-Q1
Hi Team,
Our 941 application is shown in the following figure, using one DSI0 output to 941 ,941output two FPDLINK to 948,948 output two LVDS with a resolution of 1920* 1080P@60Hz Display screen.

The I2C register configurations for 941 and 948 are as follows:

The current problem is that the display screen is blurry and flickering.
941 configure:
i2cset -f -y 1 0x0c 0x01 0x08 b
i2cset -f -y 1 0x0c 0x66 0x1A b
i2cset -f -y 1 0x0c 0x67 0x09 b
i2cset -f -y 1 0x0c 0x66 0x03 b
i2cset -f -y 1 0x0c 0x67 0x50 b
i2cset -f -y 1 0x0c 0x66 0x04 b
i2cset -f -y 1 0x0c 0x67 0x10 b
i2cset -f -y 1 0x0c 0x66 0x05 b
i2cset -f -y 1 0x0c 0x67 0x88 b
i2cset -f -y 1 0x0c 0x66 0x06 b
i2cset -f -y 1 0x0c 0x67 0x2F b
i2cset -f -y 1 0x0c 0x66 0x07 b
i2cset -f -y 1 0x0c 0x67 0x80 b
i2cset -f -y 1 0x0c 0x66 0x08 b
i2cset -f -y 1 0x0c 0x67 0x07 b
i2cset -f -y 1 0x0c 0x66 0x09 b
i2cset -f -y 1 0x0c 0x67 0x2D b
i2cset -f -y 1 0x0c 0x66 0x0A b
i2cset -f -y 1 0x0c 0x67 0x0C b
i2cset -f -y 1 0x0c 0x66 0x0B b
i2cset -f -y 1 0x0c 0x67 0x03 b
i2cset -f -y 1 0x0c 0x66 0x0C b
i2cset -f -y 1 0x0c 0x67 0x20 b
i2cset -f -y 1 0x0c 0x66 0x0D b
i2cset -f -y 1 0x0c 0x67 0x18 b
i2cset -f -y 1 0x0c 0x65 0x04 b
i2cset -f -y 1 0x0c 0x64 0x25 b
i2cset -f -y 1 0x0c 0x01 0x00 b
SOC DSI configure:
Resolution:1920x1080
Hsync:118
Hback:200
Hfront:4
Vsync:2
Vback:100
Vfront:38
framerate:60fps
dsi clk: 984M/2 = 498M (The DSI input clk is 498M for both positive and negative)
Could you help check this case? Thanks.
Best Regards,
Cherry