Part Number: PCA9548A
36. I2C Switch.pdf45. VDD_3V3.pdf
1. When we frequently access the two channels of PCA9548APWR through I2C, when accessing the two channels, the three channels will be opened with probability, and the waveform is shown in the following figure,
The yellow and blue waveforms above measure the front-end I2C signal of PCA9548APWR, while the red and green waveforms below measure the 3-channel back-end I2C signal of PCA9548APWR. From the waveform, it can be seen that the instruction we sent to PCA9548APWR (address 0x71) is to open 2 channels. May I ask why 3 channels were opened?

2. In addition, we simultaneously tested the backend signals of channels 2 and 3 of PCA9548APWR and found that channels 2 and 3 can be opened simultaneously at certain times. Is this situation caused by frequent operations on PCA9548APWR?