Part Number: LMH0340
Other Parts Discussed in Thread: LM340,
Hello teams,
Could you pls help me review the schemetic of LMH0340SQE, thanks !

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
Schematic looks fine. A couple of minor comments:
1). D229: This lightening protection part may affect return loss/eye diagram. Perhaps when you get your board back you can load and unload this part to observe the effects.
2). I am assuming there are pull up Resistors on SDA and SCK and these are not shown in the schematic.
Regards, Nasser
Hello Nasser,
One more another question. According to datasheet "Table 1. Feature Table", my chip LM340 do not support DVB-ASI, and what do we need to config the pin 6?
And , my FPGA output is 1.8V level, is it conpitable for TXCLK or TX0~4?
Thanks!
Greetings,
1). LMH0340 supports all modes including DVB-ASI. If you do not need to support DVB-ASI, then you can make this pin L"" - as noted in pin description table.
2). 1.8V common mode voltage is fine. Device common LVDS input common mode voltage is between 0.05 to 2.4V.
Regards, Nasser