Part Number: ESDS302
Other Parts Discussed in Thread: ESDS314, , DP83822I, ESDS304
Dear Specialists,
My customer is considering ESDS302 and ESDS314.
They have a question about
---
Could you please tell us know the following question about the diode with Vrwm=3.6V.
・Currently, I am using DP83822I with a power supply voltage of 3.3V.
I checked the single-end voltage of TX/RX on the device.
The output ranges from a minimum of 2V to a maximum of around 4V, centered around 3.3V.
(Basically it operates like outputting 3.3V±0.5V.)
A significant portion of the waveform is above 3.6V

In this case, what kind of problems will occur when using ESDS302 and ESDS314 (Vrwm=3.6V) under the above conditions?
When the voltage exceeds 3.6V, the current will flow to GND via the diode.
Will there be any deterioration in waveform quality or negative impact on compliance tests?
---
I appreciate your great help in advance.
Best regards,
Shinichi