Part Number: DS90UB933-Q1
Hello friends,
Can ds90ub933-q1 transmit 2M (1920*1080, 30 frames) video? The BPS of 2M_30 frames is the same as 1M_60 frames.
Best Regards
Yuan Da
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB933-Q1
Hello friends,
Can ds90ub933-q1 transmit 2M (1920*1080, 30 frames) video? The BPS of 2M_30 frames is the same as 1M_60 frames.
Best Regards
Yuan Da
Hello,
Thank you for your question. The DS90UB933 can support a pixel clock of up to 100MHz. Based on the resolution you provided the DS90UB933 will likely be able to support this video depending on the data type used (primarily the bits per pixel). You can use the attached tool to calculate the pixel clock and bandwidth required for any system configuration as well as what devices are able to support the specific configuration. For the DS90UB933, please use the "Parallel DVP (LVCMOS) Imager" tab.
2555.TI Imager-Serializer Data Rate Calculator v2.1 -- Non-NDA.xlsx
Regards,
Darrah