This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS171: TMDS TO CML

Part Number: TMDS171

Hello,

I want to interface the TMDS171 dff output to a CML logic acceptable device.

Is it necessary to add  pullup 50 ohm to 3.3 externally or  pullup 50 ohm to 3.3 exists internally in the TMDS171 transmitter output?

The differntial channels are high speed communication (2.5Gbps per lane) and I am afraid that the addition of the pullup res will affect on the signal integrity    

Thank you

Einav