This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0001: Output impedance and why the 75-ohm resistors are required

Part Number: LMH0001


Hi,

I'm looking at the main application circuit in the datasheet

1. Can you help me understand what the output impedance is of LMH0001?

2. It appears that two of the 75-ohm are being used as series termination resistors, is that correct?

3. Why are there two more 75-ohm resistors tied to VCC? What do they achieve?

4. What do the two 5.6nH inductors do?


Thanks in advance!