Part Number: SN55116
We are using SNJ55116J differential line transceiver. we use the A-B input, one input has the option 130 ohm termination at pin 6 which we do not use.
There is an internal resistor of 8K ohms sourced from Vcc to pull up the input on pin 7. Our circuit has a voltage dived network setup to prove 500 mV at pin 7. When the application was designed, I don't think the engineers took into consideration the internal 8K to Vcc. This pushed 5 500mV reference up to 600mV and varies from IC to IC. I get inconstant result when replacing IC's across date codes.
My question is:
What is the tolerance of the Nominal 8K internal resistance?
Has the SNJ55116J been revised over the years which might change this 8K resistance pull up?