This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: troubleshoot: lock and pass OK but no video link

Part Number: DS90UB954-Q1

Hello, 

We have a few functioning serdes systems and few not functioning.

what would be a good way to diagnose the non-functing units?

-observations

rails are OK 3.3, 1.8 1.1V

pass & lock are ok

I2C is working as is the bi-directional GPIOs are ok 

image does stream

-About our setup

ISP Raspberry CM4

15m cable

TSER954/953

Camera IMX477

what are the status registers we should read or changes we can make? 

Best.

  • Hello Andrew,

    can you get the values for the following registers, from a working system and a non-working system?

    953 Diagnostic registers: 0x02-0x07, 0x10-0x11, 0x32, 0x37, 0x50-0x52, 0x55, 0x56, 0x5B-0x64

    954 Diagnostic registers: 0x02-0x06, 0x1F-0x24, 0x33-0x37, 0x40-0x49, 0x4C-0x58, 0x5B-0x6D, 0x70-0x76, 0x7A-0x7C, 0xD2-0xDB.

    Also, can you provide the actual schematic for both devices, SER and DES.

    Which clocking mode is used? and what is the oscillator value on both sides?

    What type of cable are you using, and what is the length?

    Have you tried a different cable type/ length?

  • Registers readings are attached, one for a working unit and one that has the issue.

    We are operating in synchronous, 25 MHz is our crystal.

    we have a 15m and a 1m LMR195, same result regardless of length.

    -no image-

    dest action address payload Decimal Hex Binary
    d r 0x02 0 30 0x1e 0b00011110
    d r 0x03 0 32 0x20 0b00100000
    d r 0x04 0 223 0xdf 0b11011111
    d r 0x05 0 1 0x01 0b00000001
    d r 0x06 0 0 0x00 0b00000000
    d r 0x1F 0 0 0x00 0b00000000
    d r 0x20 0 32 0x20 0b00100000
    d r 0x21 0 1 0x01 0b00000001
    d r 0x22 0 0 0x00 0b00000000
    d r 0x23 0 0 0x00 0b00000000
    d r 0x24 0 0 0x00 0b00000000
    d r 0x33 0 97 0x61 0b01100001
    d r 0x34 0 64 0x40 0b01000000
    d r 0x35 0 1 0x01 0b00000001
    d r 0x36 0 0 0x00 0b00000000
    d r 0x37 0 1 0x01 0b00000001
    d r 0x40 0 0 0x00 0b00000000
    d r 0x41 0 167 0xa7 0b10100111
    d r 0x42 0 113 0x71 0b01110001
    d r 0x43 0 1 0x01 0b00000001
    d r 0x44 0 0 0x00 0b00000000
    d r 0x45 0 0 0x00 0b00000000
    d r 0x46 0 0 0x00 0b00000000
    d r 0x47 0 0 0x00 0b00000000
    d r 0x48 0 0 0x00 0b00000000
    d r 0x49 0 0 0x00 0b00000000
    d r 0x4C 0 1 0x01 0b00000001
    d r 0x4D 0 3 0x03 0b00000011
    d r 0x4E 0 69 0x45 0b01000101
    d r 0x4F 0 100 0x64 0b01100100
    d r 0x50 0 0 0x00 0b00000000
    d r 0x51 0 0 0x00 0b00000000
    d r 0x52 0 0 0x00 0b00000000
    d r 0x53 0 3 0x03 0b00000011
    d r 0x54 0 0 0x00 0b00000000
    d r 0x55 0 0 0x00 0b00000000
    d r 0x56 0 0 0x00 0b00000000
    d r 0x57 0 0 0x00 0b00000000
    d r 0x58 0 94 0x5e 0b01011110
    d r 0x5B 0 48 0x30 0b00110000
    d r 0x5C 0 48 0x30 0b00110000
    d r 0x5D 0 52 0x34 0b00110100
    d r 0x5E 0 200 0xc8 0b11001000
    d r 0x5F 0 0 0x00 0b00000000
    d r 0x61 0 0 0x00 0b00000000
    d r 0x62 0 0 0x00 0b00000000
    d r 0x63 0 0 0x00 0b00000000
    d r 0x64 0 0 0x00 0b00000000
    d r 0x65 0 52 0x34 0b00110100
    d r 0x66 0 200 0xc8 0b11001000
    d r 0x67 0 0 0x00 0b00000000
    d r 0x68 0 0 0x00 0b00000000
    d r 0x69 0 0 0x00 0b00000000
    d r 0x6A 0 0 0x00 0b00000000
    d r 0x6B 0 0 0x00 0b00000000
    d r 0x6C 0 0 0x00 0b00000000
    d r 0x6D 0 124 0x7c 0b01111100
    d r 0x70 0 43 0x2b 0b00101011
    d r 0x71 0 44 0x2c 0b00101100
    d r 0x72 0 228 0xe4 0b11100100
    d r 0x73 0 4 0x04 0b00000100
    d r 0x74 0 58 0x3a 0b00111010
    d r 0x75 0 11 0x0b 0b00001011
    d r 0x76 0 226 0xe2 0b11100010
    d r 0x7A 0 0 0x00 0b00000000
    d r 0x7B 0 0 0x00 0b00000000
    d r 0x7C 0 32 0x20 0b00100000
    d r 0xD2 0 148 0x94 0b10010100
    d r 0xD3 0 4 0x04 0b00000100
    d r 0xD4 0 96 0x60 0b01100000
    d r 0xD5 0 242 0xf2 0b11110010
    d r 0xD6 0 0 0x00 0b00000000
    d r 0xD7 0 0 0x00 0b00000000
    d r 0xD8 0 0 0x00 0b00000000
    d r 0xD9 0 0 0x00 0b00000000
    d r 0xDA 0 0 0x00 0b00000000
    d r 0xDB 0 0 0x00 0b00000000
    s r 0x02 0 19 0x13 0b00010011
    s r 0x03 0 72 0x48 0b01001000
    s r 0x04 0 0 0x00 0b00000000
    s r 0x05 0 3 0x03 0b00000011
    s r 0x06 0 65 0x41 0b01000001
    s r 0x07 0 40 0x28 0b00101000
    s r 0x10 0 0 0x00 0b00000000
    s r 0x11 0 0 0x00 0b00000000
    s r 0x32 0 136 0x88 0b10001000
    s r 0x37 0 96 0x60 0b01100000
    s r 0x50 0 32 0x20 0b00100000
    s r 0x51 0 192 0xc0 0b11000000
    s r 0x52 0 69 0x45 0b01000101
    s r 0x55 0 0 0x00 0b00000000
    s r 0x56 0 0 0x00 0b00000000
    s r 0x5B 0 0 0x00 0b00000000
    s r 0x5C 0 0 0x00 0b00000000
    s r 0x5D 0 0 0x00 0b00000000
    s r 0x5E 0 0 0x00 0b00000000
    s r 0x5F 0 0 0x00 0b00000000
    s r 0x60 0 0 0x00 0b00000000
    s r 0x61 0 18 0x12 0b00010010
    s r 0x62 0 226 0xe2 0b11100010
    s r 0x63 0 11 0x0b 0b00001011
    s r 0x64 0 16 0x10

    0b00010000

    -image works-

    dest action address payload Decimal Hex Binary
    d r 0x02 0 30 0x1e 0b00011110
    d r 0x03 0 32 0x20 0b00100000
    d r 0x04 0 223 0xdf 0b11011111
    d r 0x05 0 1 0x01 0b00000001
    d r 0x06 0 0 0x00 0b00000000
    d r 0x1F 0 0 0x00 0b00000000
    d r 0x20 0 32 0x20 0b00100000
    d r 0x21 0 1 0x01 0b00000001
    d r 0x22 0 0 0x00 0b00000000
    d r 0x23 0 0 0x00 0b00000000
    d r 0x24 0 0 0x00 0b00000000
    d r 0x33 0 97 0x61 0b01100001
    d r 0x34 0 64 0x40 0b01000000
    d r 0x35 0 1 0x01 0b00000001
    d r 0x36 0 0 0x00 0b00000000
    d r 0x37 0 1 0x01 0b00000001
    d r 0x40 0 0 0x00 0b00000000
    d r 0x41 0 167 0xa7 0b10100111
    d r 0x42 0 113 0x71 0b01110001
    d r 0x43 0 1 0x01 0b00000001
    d r 0x44 0 0 0x00 0b00000000
    d r 0x45 0 0 0x00 0b00000000
    d r 0x46 0 0 0x00 0b00000000
    d r 0x47 0 0 0x00 0b00000000
    d r 0x48 0 0 0x00 0b00000000
    d r 0x49 0 0 0x00 0b00000000
    d r 0x4C 0 1 0x01 0b00000001
    d r 0x4D 0 3 0x03 0b00000011
    d r 0x4E 0 69 0x45 0b01000101
    d r 0x4F 0 100 0x64 0b01100100
    d r 0x50 0 0 0x00 0b00000000
    d r 0x51 0 0 0x00 0b00000000
    d r 0x52 0 0 0x00 0b00000000
    d r 0x53 0 3 0x03 0b00000011
    d r 0x54 0 0 0x00 0b00000000
    d r 0x55 0 0 0x00 0b00000000
    d r 0x56 0 0 0x00 0b00000000
    d r 0x57 0 0 0x00 0b00000000
    d r 0x58 0 94 0x5e 0b01011110
    d r 0x5B 0 48 0x30 0b00110000
    d r 0x5C 0 48 0x30 0b00110000
    d r 0x5D 0 52 0x34 0b00110100
    d r 0x5E 0 200 0xc8 0b11001000
    d r 0x5F 0 0 0x00 0b00000000
    d r 0x61 0 0 0x00 0b00000000
    d r 0x62 0 0 0x00 0b00000000
    d r 0x63 0 0 0x00 0b00000000
    d r 0x64 0 0 0x00 0b00000000
    d r 0x65 0 52 0x34 0b00110100
    d r 0x66 0 200 0xc8 0b11001000
    d r 0x67 0 0 0x00 0b00000000
    d r 0x68 0 0 0x00 0b00000000
    d r 0x69 0 0 0x00 0b00000000
    d r 0x6A 0 0 0x00 0b00000000
    d r 0x6B 0 0 0x00 0b00000000
    d r 0x6C 0 0 0x00 0b00000000
    d r 0x6D 0 124 0x7c 0b01111100
    d r 0x70 0 43 0x2b 0b00101011
    d r 0x71 0 44 0x2c 0b00101100
    d r 0x72 0 228 0xe4 0b11100100
    d r 0x73 0 4 0x04 0b00000100
    d r 0x74 0 58 0x3a 0b00111010
    d r 0x75 0 11 0x0b 0b00001011
    d r 0x76 0 226 0xe2 0b11100010
    d r 0x7A 0 0 0x00 0b00000000
    d r 0x7B 0 0 0x00 0b00000000
    d r 0x7C 0 32 0x20 0b00100000
    d r 0xD2 0 148 0x94 0b10010100
    d r 0xD3 0 4 0x04 0b00000100
    d r 0xD4 0 96 0x60 0b01100000
    d r 0xD5 0 242 0xf2 0b11110010
    d r 0xD6 0 0 0x00 0b00000000
    d r 0xD7 0 0 0x00 0b00000000
    d r 0xD8 0 0 0x00 0b00000000
    d r 0xD9 0 0 0x00 0b00000000
    d r 0xDA 0 0 0x00 0b00000000
    d r 0xDB 0 0 0x00 0b00000000
    s r 0x02 0 19 0x13 0b00010011
    s r 0x03 0 72 0x48 0b01001000
    s r 0x04 0 0 0x00 0b00000000
    s r 0x05 0 3 0x03 0b00000011
    s r 0x06 0 65 0x41 0b01000001
    s r 0x07 0 40 0x28 0b00101000
    s r 0x10 0 0 0x00 0b00000000
    s r 0x11 0 0 0x00 0b00000000
    s r 0x32 0 136 0x88 0b10001000
    s r 0x37 0 96 0x60 0b01100000
    s r 0x50 0 32 0x20 0b00100000
    s r 0x51 0 192 0xc0 0b11000000
    s r 0x52 0 101 0x65 0b01100101
    s r 0x55 0 0 0x00 0b00000000
    s r 0x56 0 0 0x00 0b00000000
    s r 0x5B 0 0 0x00 0b00000000
    s r 0x5C 0 0 0x00 0b00000000
    s r 0x5D 0 0 0x00 0b00000000
    s r 0x5E 0 0 0x00 0b00000000
    s r 0x5F 0 0 0x00 0b00000000
    s r 0x60 0 0 0x00 0b00000000
    s r 0x61 0 18 0x12 0b00010010
    s r 0x62 0 226 0xe2 0b11100010
    s r 0x63 0 11 0x0b 0b00001011
    s r 0x64 0 16 0x10 0b00010000
  • Hello Andrew,

    I have compared both register dumps. In both cases the DES is receiving the exact same data, and this is being sent to the DES CSI-2 TX output. Please double check your setup after the DES.