Part Number: TCAN1146-Q1
I am using CAN Transceiver TCAN1146-Q1 with functionality of INH to control the power supply of the MCU.
INH pin is configured to be 300ms low when there is a WDG failure.
I have a corner case where TCAN1146-Q1 enters in a state where INH is always low: I configure the WDG in window mode and on a diagnostic command I trigger WDG twice to force a reset. Right after I set the WDG in OFF mode.
Even if TCAN1146-Q1 is in Fail state, INH pin should still be high.
Could you please test this on your side and give a feedback why this is happening?