Part Number: TCA6408A-Q1
Dear TI experts,
My customer made their first schematic with TCA6408A-Q1. Could you review the schematic below?

Best regards,
Chase
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA6408A-Q1
Dear TI experts,
My customer made their first schematic with TCA6408A-Q1. Could you review the schematic below?

Best regards,
Chase
Hi Chase,
| Check | Comments (If Needed) |
| Local Decoupling Capacitors |
100 nF decoupling capacitors present on the VCCP and VCCI supply lines. These are good values |
| Verify the schematic pinout matches the data sheet pinout. | Correct |
| Verify that the SDA, and SCL net names match SDA and SCL pinout. | Correct |
| Check that the pullup resistors are present on the SDA and SCL net within the schematic. | Pull-up resistors are required. I am assuming these are in another page of the schematic. |
| Unused GPIO pins are biased to either VCC or GND via resistor. | No unused GPIO pins |
| Device address is unique on the bus unless using an I2C switch or I2C MUX to resolve conflicts. | ADDR pin correctly connected to GND |
| If the device has a #RESET pin, bias the pin high (preferably with a pullup resistor) after powering up | R8919 is a very strong pull-up resistor at 22ohm. I don't think the external GPIO would be able to drive this pin LOW if it needed to conduct and external /RESET condition? Is this a problem for the implementation? |
| If the device has a #INT pin and the #INT pin is used, tie this pin to a pullup resistor. | Interrupt pin is corrected connected to pull-up resistor to the supply voltage. |
Regards,
Tyler