Part Number: TMDS171
Other Parts Discussed in Thread: TMDS181
Hello, I have a question about using TMDS171.
I am using two TMDS171 devices in a single channel, with each device handling three of the six TMDS inputs, to accommodate a total of six TMDS inputs.
I'm using the clock signal of the TMDS inputs from the master TMDS171 as inputs, feeding the master output into the slave input, and using the slave output as the final output.
It appears that when using TMDS dual, the clock signal output from the master differs from the input clock signal.
Is there a solution to using pinstrap mode?