Hello
I am using the TI913 & TI914 serdes.
The HW is as follow:
- image sensor --> TI913 --> Fakra cable --> TI914 --> ISP.
According to some ISP's registers, the signal which is arriving at the ISP is unstable.
Which registers on the TI914 (and also Ti913) should be monitored to check that the quality signal which is going out from the TI914 is OK?
Thanks,
Muriel