This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044AV-Q1: ISO 11898-1

Part Number: TCAN1044AV-Q1


Hi expert,

May I know if TCAN1044 certified the ISO 11898-1 standard? 

Also is there CAN-FD number of device allowed restriction? 

Thanks,

Allan

  • Allan,

    TCAN1044AV-Q1 is compliant with ISO 11898-2, as this is the physical layer definition and TCAN1044AV-Q1 is just that, a physical layer transceiver.

    ISO 11898-1 is the data link definition, not necessarily relevant to the TCAN1044AV-Q1.

    Please let us know if you have any other questions.

    Regards,

    Eric Hackett