Part Number: AM26C31
Other Parts Discussed in Thread: AM26LV31E, AM2631
hi,
We are using an incremental encoder in our product.
The encoder supplier is using AM26C31.
In our motion control board, the interface schematic to the encoder is shown below.

The good encoder counts for a fixed distance travel is given below (QA, QB) . It gives 50.456K rising edges if we see the events in right edge of the screen shot..

Some faulty units we are seeing encoder pulses missing
For the faulty encoder, the screen shot is given below. It gives only 18.742K rising edges if we see the events in right edge of the screen shot.. But the motor is moved to the same distance and confirmed it using laser distance sensor.

So it is clear that the IC AM26C31 in the encoder module is not behaving.
This could be due to long term failure or some thing as the units were running properly and it had developed these issues now.
The receiver interface circuit above is right. Is there anything that could harm AM26C31?
Your inputs are valuable as the production is stuck due to this issue.
regards
Subramani