Part Number: TUSB8041
Other Parts Discussed in Thread: HD3SS6126
Hi Team,
Customer is having USB 3.0 MUX requirements .Refer the below block diagram.
The HS & SS signals are the inputs to Mux from Processor or Host controller. They prefer to use one common USB 3.0 port to switch between the direct SS & HS signal (Processor) or from the USB 3.0 HUB. It requires to short or develop a stub at the output of the MUX & USB 3.0 connector.
Customer required inputs from us that the stub or junction between the USB connector and MUX would not deviate the requirements?
When A port is selected what would be status of B port ? will it be in Hi-Z state?
Do advice if the below configuration would meet the requirements.

Regards, S Mathew.