Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: DP83TD510E,
- You have two DP83TD510E-EVM boards. The DP83TD510E is a Single Pair Ethernet (SPE) PHY device from Texas Instruments designed to transmit Ethernet frames over a single twisted pair.
- The first DP83TD510E-EVM board:
- Ethernet side (RJ45) is connected to your laptop.
- SPE (Single Pair Ethernet) side is connected to the second DP83TD510E-EVM board.
- The second DP83TD510E-EVM board:
- SPE side is connected to the first DP83TD510E-EVM board.
- Ethernet side (RJ45) is connected to your PC.
- You then try to ping the IP address of the PC.
Laptop -> EVM Board 1 -> EVM Board 2 -> PC
Will communication still happen if i remove the MSP340?

this is essential my setup , I didn't power the board in this instance but, when I do the led that appear when you plug in your ethernet port on the rj45 side doesn't light up anymore and the computer says Im not connected to anything.