Part Number: TUSB9261-Q1
Other Parts Discussed in Thread: TUSB9261
Hi,
There are some GPIO pins in the datasheet that are said to be assigned to default settings which are given in Table 8 (GPIO/PWM LED Designations). Is there a default firmware on the chip OR are these settings loaded after flashing drivers to the chip via USB?
Also is it normal "to be not detected" of the chip or any related USB node from a linux or a windows host, if there is not any software that can recognize the chip?
We have a custom board in which TUSB9261-Q1 exists, however it is not being detected by either windows or linux(ubuntu). What can be the reason?
Best Regards,
Mustafa