Part Number: TCAN1043-Q1
Hi experts
Our customer is using TCAN1043-Q1 in their system, and they use INH to enable/disable the LDO for VCC/VIO. But we found a potential issue here is:
When the VBAT drops to about 4.2V(It may not trigger UVsup), but it may trigger UVCC since there is ~200mV dropout voltage through LDO. In this case, TCAN1043-Q1 will enter sleep mode and INH goes to Hi-Z, which will disable the LDO.

When Vsup recover from this point(no UVsup), it will not be a cold start and TCAN1043-Q1 stays in sleep mode. Only WUP can wake up the device.
Our point is, do we have any workarounds to avoid this issue? OEM asks for staying standby mode instead of Sleep mode when the VBAT recovers.
One way from our side is to change the power rail, use SEPIC/buck-boost to generate the VCC, it will make VCC stable even Vsup is lower than VCC. But we want your insights, expect for your reply, thanks!