Part Number: DP83620
Hi Experts,
In our Project, we are using DP83620SQE/NOPB Ethernet Transceiver (RMII mode). During DVT Testing of Ethernet section, We have identified failure in MDC to MDIO (output) Delay Time with respect to Datasheet.

- Instead of Max delay time of 20ns we are observed 413ns Delay time. Please find the attached image for your analysis.

- We have also observed the MDC Clock as 650.1kHz. Please find the attached image. (As per Datasheet MDC Frequency: Typ 2.5MHz to Max 25MHz)

1. We are suspecting the MDC to MDIO Higher time delay because of MDC Clock is very low (700khz). Compared to Typ 2.5MHz to 25MHz they have mentioned. Please let us know is that true?
2. As we checked the MDC Clock is TI Driver based and fixed, seems it couldn't be configured to 25MHz. Is there any option to increase the MDC Clock frequency to 25MHz as mentioned in Section 4.7 Table?
Please provide inputs on the same
Thanks and Regards,
Palanikumar E