Part Number: P82B96
Thank you for your help.
Please tell me about the VOL regulations and IOL regulations regarding P82B96.
Note (5) on page 8 of the P82B96 data sheet contains the following information.
"(5) The minimum value requirement for pullup current, 200 μA, ensures that the minimum value for VSX output low always exceeds the minimum VSx input high level to eliminate any possibility of latching.
" Please tell me the meaning of the above sentence. Does this mean that ``at least 200 μA must flow through the IOL at all times?''
Or is this not a problem as long as the SX terminals of multiple P82B96s are not directly connected?
The characteristics diagram of VOL is shown in Figure 1 and Figure 2 on page 11 of the data sheet.
The data sheet only mentions IOLs of 0.2mA and 3mA, but are there any VOL characteristics for current values between 0.2mA and 3mA?
Also, is it correct to think that the characteristics of VOL depend on the ON resistance of the internal FET and are proportional to the magnitude of the IOL current value?