Part Number: DS320PR1601RSCEVM
Other Parts Discussed in Thread: USB2ANY, , DS320PR1601
Hi,
1. can we program the redriver via sm bus using adapter cards other than usb2any or aardvark?
2. do eeprom also need above said adapter cards?
3. in DS320PR1601RSCEVM design file there are two signals namely scl_c and scl , sda_c and sda going to pin b5 and b6 of pciex16 connector.
a) do r78 and r79 are placed in final design?
b) if so is there any issue when two scl/sda going to one pin?
Thanks and Regards,
Shekha Shoukath