This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for a specific USB HUB controller

Hello everyone,

I am reaching out because I am in search of a USB HUB controller (1 to 4) that allows for the locking of ports according to a predetermined priority order. If the HUB has 4 output ports, I would like to be able to statically assign port 1 to a specific device, port 2 to another, port 3 to a third, and port 4 to a fourth device. I want this configuration to remain constant, unlike a gaming console where the assignment order of controllers can vary based on their connection. In other words, I want to ensure that the device connected to port 1 always remains device number 1, regardless of the order in which devices are plugged in. Do you have a component capable of managing this functionality?

Thank by advance and best regards,

Maurice